mipi

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mipi

1,668 Views
sumosumo
Contributor I

hi imx community

i have ov5640 mipi of econsystem and i found that the driver (ov5640_mipi of 3.10.17 kernel) doesnt contain any registers configuration for hdmi.

did anyone managed to use hdmi anyhow with the driver mentioned above?

thanks!

0 Kudos
Reply
1 Reply

1,560 Views
igorpadykov
NXP Employee
NXP Employee

Hi sumo

for hdmi input one can use parallel input (csi), for input through mipi one will have

to use additional external converter and modify sources, as below :

Some Experience When Enable MIPI Camera

https://community.freescale.com/thread/314211

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply