Hi ,
I have MCIMXABASEV1 with imx6dl CPU card , I would like to know which microphone is suitable for the above mentioned baseboard.
Please share the suitable links.
Thanks in advance .
Abhirup Mitra
Unfortunately i.MX6 processors has no analog microphone input.
However it has SSI interface that supports I2S mode. So you can use to connect I2S microphone.
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I agree with you Victor but as I already mentioned , I have baseboard which has got microphone-in as well as audio-in & out ports.
I connected microphone in the RCA jacks, but am not able to record anything.
As you can see, we don't have a suitable microphone for the jacks which may be one reason for the problem.
Please give a solution for this!
Thanks ,
Abhirup
What is the model number of the board that plugs in the microphone? Thank you!