mfgtool vs MIMXRT1051CVL5B

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mfgtool vs MIMXRT1051CVL5B

1,791件の閲覧回数
ffloree
Contributor III

did someone verify Flashloader_RT1050_1.1 on MIMXRT1051CVL5B? it seems that after loading ivt_flashloader.bin, HID device lost, then stuck at "No Device Connected", see the script:

<LIST name="MXRT105x-DevBoot" desc="Manufacturing with Flashloader">
<!-- Stage 1, load and execute Flashloader -->
<CMD state="BootStrap" type="boot" body="BootStrap" file="ivt_flashloader.bin" > Loading Flashloader. </CMD>
<CMD state="BootStrap" type="jump" onError = "ignore"> Jumping to Flashloader. </CMD>

## stuck here!!

<!-- Stage 2, Program boot image into external memory using Flashloader -->
<CMD state="Blhost" type="blhost" body="get-property 1" > Get Property 1. </CMD> <!--Used to test if flashloader runs successfully-->
<CMD state="Blhost" type="blhost" timeout="95000" body="receive-sb-file \"Profiles\\MXRT105X\\OS Firmware\\boot_image.sb\"" > Program Boot image </CMD>
<CMD state="Blhost" type="blhost" body="Update Completed!">Done</CMD>
</LIST>

タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,563件の閲覧回数
jay_heng
NXP Employee
NXP Employee

You can try this GUI tool, it is same as MfgTool, but more powerful

Releases · JayHeng/RT-Flash · GitHub

0 件の賞賛
返信

1,563件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi tom

if this is custom board one can check clocks, in particular 24MHz and its stability,

please check Hardware Development Guide for the MIMXRT1050 Processor
https://www.nxp.com/docs/en/user-guide/MIMXRT1050EVKHUG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信