mfgtool auto close when detect a device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mfgtool auto close when detect a device

2,814 Views
347653194
Contributor II

I want to download android 7.1 and 8.0 demo bsp to sabresd board,mfgtool open after vbs script run,but it will auto close when the board connect to computer,my OS is windows 10,I remember it was work normally in XP,what is the reason why?

Tags (1)
0 Kudos
Reply
4 Replies

2,802 Views
disheng
Contributor III

you can check the MfgTool.log in the root folder

0 Kudos
Reply

2,739 Views
347653194
Contributor II

it is the log

0 Kudos
Reply

2,810 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which board are you using?

0 Kudos
Reply

2,758 Views
347653194
Contributor II

imx6q-sabresd-sdp

Tags (1)
0 Kudos
Reply