mfgtool auto close when detect a device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mfgtool auto close when detect a device

2,750件の閲覧回数
347653194
Contributor II

I want to download android 7.1 and 8.0 demo bsp to sabresd board,mfgtool open after vbs script run,but it will auto close when the board connect to computer,my OS is windows 10,I remember it was work normally in XP,what is the reason why?

タグ(1)
0 件の賞賛
返信
4 返答(返信)

2,738件の閲覧回数
disheng
Contributor III

you can check the MfgTool.log in the root folder

0 件の賞賛
返信

2,675件の閲覧回数
347653194
Contributor II

it is the log

0 件の賞賛
返信

2,746件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Which board are you using?

0 件の賞賛
返信

2,694件の閲覧回数
347653194
Contributor II

imx6q-sabresd-sdp

タグ(1)
0 件の賞賛
返信