mfgtool, No Device Connected.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mfgtool, No Device Connected.

2,087 Views
openclosed
Contributor I

Hi.

I have an i.mx6qp sabred board and I want to download it using mfgtool.
However, the PC does not recognize the device.
SW6 dip switch is set to 00001100.
When a USB OTB connector is connected to a PC, it is recognized as SE Blank ARIK HID.
If you try to force reinstallation with mfgtools \ Drivers \ iMX_BulkIO_Driver \ imxusb.inf, the installation will fail because it is not 64-bit compatible.
The MFG tool version is 2.7.0.
What should I do?

Labels (3)
Tags (1)
0 Kudos
Reply
1 Reply

2,016 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Is your board win7 or win10 system? And which version BSP are you using?

0 Kudos
Reply