menuconfig

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

menuconfig

2,369件の閲覧回数
santhosha
Contributor II

How to get the menuconfig to enable/disable the required drivers?

Will bitbake linux-imx -c menuconfig helps?

ラベル(1)
2 返答(返信)

2,170件の閲覧回数
aravinthkumarja
Senior Contributor II

Hi santhosha​,

Run the menuconfig command:

=> bitbake linux-yocto -c menuconfig

For your Reference:

Yocto Project Linux Kernel Development Manual

2,170件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Thanks, Aravinthkumar Jayaprakasam!

I would also recommend looking at the following Yocto Tutorial where the kernel is configured outside of bitbake, which is useful in some circunstances.

Yocto Training - Task #5

You may need to use a different kernel recipe depending on which Release of the BSP or Branch from the FSL Community BSP you are using.

Regards,

0 件の賞賛
返信