on a custom board, the memtool reading IPU1 and IPU2 and VDOA modules hangs. Most other modules work fine.
[root@freescale home]# ./memtool IPU1.*
./memtool IPU1.*
SOC is mx6q
IPU1 Addr:0x2400000
I did enabled the all clocks as Yuri said, using the following lines:
./memtool 0x020c4068=0xffffffff
./memtool 0x020c406c=0xffffffff
./memtool 0x020c4070=0xffffffff
./memtool 0x020c4074=0xffffffff
./memtool 0x020c4078=0xffffffff
./memtool 0x020c407c=0xffffffff
./memtool 0x020c4080=0xffffffff
thanks a lot!
Hi Oufei
clock gating is described in sect.18.6.23 CCM Clock Gating Register 0 (CCM_CCGR0)
i.MX6DQ Reference Manual
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf
what BSP are you using, please try
linux-2.6-imx.git - Freescale i.MX Linux Tree
use imx-test (memtool)
www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.4.tar.gz
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
thanks igor,
I am using a file given by the chip distributor.
L3.0.35_4.1.0_130816_source
Looks like I need do a clean start from scratch. I am new to IMX.
Is yocto the officially recommended ?