make file error in mcuxpresso ide

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

make file error in mcuxpresso ide

1,635 次查看
kavyav
Contributor I

The attatched image contains error ,plz share the solution to this

0 项奖励
回复
1 回复

1,610 次查看
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @kavyav,

I hope you are doing well.

From the image, It is seen that error is with the below statement
"make -r -j4 all" terminated with exit code 2. The build might be incomplete.

I have a few queries to ask.
->Which IMX board are you using?
->Have you made any changes to Makefile or are you using the default given SDK

I have shared a link to docs please refer to section 5.1 (Build an app using Linux host) for reference only.
https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/imx-processors/132881/1/Getting%20Starte...

Thanks & Regards,
Dhruvit Vasavada

0 项奖励
回复