maaxboard mickledore branch image NO hdmi display

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

maaxboard mickledore branch image NO hdmi display

141件の閲覧回数
gonewithwind-peter
Senior Contributor I

HI all,
I just cloned
https://github.com/Avnet/meta-maaxboard/tree/mickledore a week ago,
meta-maaxboard commit is :
commit 95233e4 (HEAD -> mickledore, origin/mickledore)
Author: wenxue.guo wenxue.guo@avnet.com
Date: Wed Jan 17 14:58:12 2024 +0800

I build with avnet-image-chromium
but after image boot up , there is no any display including no any lines ,log out put in hdmi screen( the old zeus it had wayland display before ).
after bootup, I changed /boot/uEnv.txt
to
####Display can support mipi, hdmi and dual
dtoverlay_display=hdmi

it seems hdmi shoud work, but after rebooting, no any dispplay ether.
it seems the image no any output from hdmi

any help ? thanks

 

 

I also post the issue here: 

https://github.com/Avnet/meta-maaxboard/issues/9

0 件の賞賛
返信
2 返答(返信)

124件の閲覧回数
gonewithwind-peter
Senior Contributor I

solved. changed uEnv.txt in sd card the first partition (or in yocto source code) not in /boot/uEnv.txt after booting up

0 件の賞賛
返信

110件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

I'm glad you solved the issue, then you are playing with the yocto BSP from the community

Regards

0 件の賞賛
返信