mSATA on iMX8QM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mSATA on iMX8QM

959件の閲覧回数
pbain
Contributor III

Hi, looking to see if it is possible to implement an mSATA (pSLC) device on the iMX8QM. Mapping the differential TX and RX pairs is simple, but I am at a loss as to how to integrate the DEVSLP and presence detection without simply using 2xGPIO.
Will this also pose any software concerns?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

860件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Peter

for current i.MX8 sata implementation one can look at

linux/arch/arm64/boot/dts/freescale/fsl-imx8qm-mek.dtsi

fsl-imx8qm-mek.dtsi\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel 

and linux/Documentation/devicetree/bindings/ata/imx-sata.txt

imx-sata.txt\ata\bindings\devicetree\Documentation - linux-imx - i.MX Linux kernel 

for other features not listed there seems it will be necessary to add customizations.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信