ltib issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ltib issues

1,601 Views
sarathsanthoss
Contributor I

hi there,

             i'm getting the following error while running ./ltib anyone help me

ltib cannot be run because one or more of the host packages needed to run it

are either missing or out of date or not in ltib's standard path.  Please

install/upgrade these packages on your host.  If you have your own utilities

in non-standard paths, please add an entry into the .ltibrc file for example:

%path_std

/usr/local/bin:/usr/bin:/bin:/usr/bin/X11:/usr/X11R6/bin:/my/own/exes

Package                Minimum ver   Installed info

-------                -----------   ---------------

zlib                   0             not installed

Died at ./ltib line 1409.

traceback:

main::host_checks:1409

  main:554

Started: Sun Oct 18 11:13:59 2015

Ended:   Sun Oct 18 11:14:02 2015

Elapsed: 3 seconds

Build Failed

Exiting on error or interrupt

Labels (1)
0 Kudos
Reply
1 Reply

1,513 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Sarathkumar Natarajan,

I would suggest reviewing the following thread which talks about this same issue.

how to install zlib for ltib installation ..??

0 Kudos
Reply