load per cpu

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,452件の閲覧回数
niklasmolin
Senior Contributor I

Hi.

I'm using Yocto to build my linux image for a i.MX6D (2 cores).

How do I check how much load is on each core.

When I run top, it only show the total load.

Is there a way to see how much load is on each core.

Thanks,

Niklas

ラベル(3)
0 件の賞賛
返信
1 解決策
4,175件の閲覧回数
dmitrypozhidaev
Contributor III

try htop

it is more humane

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
4,176件の閲覧回数
dmitrypozhidaev
Contributor III

try htop

it is more humane

0 件の賞賛
返信
4,175件の閲覧回数
niklasmolin
Senior Contributor I

I was considering to try this command, I haven't had any time to test it yet.

0 件の賞賛
返信
4,175件の閲覧回数
b36401
NXP Employee
NXP Employee

Hello,

You can simply type "1" when you are running top utility
to see per core CPU load.

Have a great day,                                                                                                                                                                  
Victor                                                                                                                                                                             
                                                                                                                                                                                   
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
4,175件の閲覧回数
niklasmolin
Senior Contributor I

Hi Victor.

I tried "1", but nothing happens.

Could it be that it only runs on one Core?

When I do a "more /proc/cpuInfo" I can see both cores.

Thanks,

Niklas

0 件の賞賛
返信
4,175件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Niklas

I think links below answer this

Load (computing) - Wikipedia, the free encyclopedia

How do I Find Out Linux CPU Utilization? - nixCraft

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信