librsvg_2.40.20.bb do not generate the file libpixbufloader-svg.so in i.MX8MQ_EVK yocto zeus 5.4.70?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

librsvg_2.40.20.bb do not generate the file libpixbufloader-svg.so in i.MX8MQ_EVK yocto zeus 5.4.70?

1,365 Views
anhui527
Contributor III

HI, NXP experts

we use the Yocto zeus 5.4.70 to generate one image on which i run a gtk+3 application

when the application's main window is showed, the main window missed the some icons(minimized icon,maximized icon,close icon). it looks like the attached pic.you can see that there are no icons displayed at right-top corner below

window missing icons.jpg

and my gtk application use the default Adwaita theme and icon. this Adwaita theme use the svg format to render the pixbuf. so i add the librsvg_2.40.20.bb into my local.conf and re-build the image.

in result , librsvg_2.40.20.bb generate the librsvg-2.so, but ,in /usr/lib/gdk-pixbuf-2.0/2.10.0/loader/ , no libpixbufloader-svg.so which will be used by gtk.

also , we try the zeus 5.4.24 , the same result it has.

so , my question is :

in yocto zeus 5.4.70 , why the librsvg_2.40.20.bb do not generate the lib libpixbufloader-svg.so ?

 

0 Kudos
Reply
2 Replies

1,342 Views
anhui527
Contributor III

Hi,NXP experts

could you give me some advice ? thanks.

0 Kudos
Reply

1,358 Views
anhui527
Contributor III

NXP experts:

pls, is the issue i depicted above a problem ? or i understood it wrongly?

thanks

0 Kudos
Reply