libcodec and libhantro dependencies

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

libcodec and libhantro dependencies

894件の閲覧回数
Hubanys
Contributor II

FAILED: out/soong/build.ninja
cd "$(dirname "out/host/linux-x86/bin/soong_build")" && BUILDER="$PWD/$(basename "out/host/linux-x86/bin/soong_build")" && cd / && env -i "$BUILDER" --top "$TOP" --soong_out "out/soong" --out "out" -o out/soong/build.ninja --globListDir build --globFile out/soong/globs-build.ninja -t -l out/.module_paths/Android.bp.list --available_env out/soong/soong.environment.available --used_env out/soong/soong.environment.used.build Android.bp
error: vendor/nxp/vpu_wrapper/Android.bp:85:1: "lib_vpu_wrapper" depends on undefined module "libcodec"
error: vendor/nxp/vpu_wrapper/Android.bp:85:1: "lib_vpu_wrapper" depends on undefined module "libhantro"
ninja: build stopped: subcommand failed.
10:34:42 soong bootstrap failed with: exit status 1

#### failed to build some targets (17 seconds) ####

when I do “make -j4” using the common lunch “lunch evk_8mp-userdebug” then the problem appears like that, what is the solution?

ラベル(1)
0 件の賞賛
返信
1 返信

844件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

Please check the code for completeness and try again

Best Regards
Zhiming

0 件の賞賛
返信