lcd display image in different offset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lcd display image in different offset

2,293 Views
rans
Senior Contributor I

Hello,

I have configured a 240x320 LCD with timing correcpond to 240 pixel line and 512 lines (instead of 320). Any other configuration did not work with my LCD.

Now I can finally get a stable image , but each time the image starts at different line (and the rest of the screen is blank).

on doing:

dd if=/dev/zero of=/dev/fb0

It resolved this issue.

Does anyone anyone knows why the above command resolve the problem ? I would assume that framebuffer content is the same even before doing this command, so i don't understand the effect.

I also do not understand what the reason for the different line offset in the first place.

Thanks,

Ran

0 Kudos
Reply
4 Replies

2,192 Views
Yuri
NXP Employee
NXP Employee

Hello,

Looks like the LCD was not fully correctly in initialized.

Please look at app note  AN3974 “Different Display Configurations on

i.MX35 Linux PDK” describing display parameters for initialization.

http://cache.freescale.com/files/dsp/doc/app_note/AN3974.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,192 Views
rans
Senior Contributor I

Hi Yuri,

Thank you for the suggestion and link.

But why did the following command seems to redsolved the issue

dd if=/dev/zero of=/dev/fb0

What effect does it have, and does it imply that the timing are correct ?

Regards,

Ran

0 Kudos
Reply

2,192 Views
rans
Senior Contributor I

Hi,

I wanted to add that framebuffer is configured as following:

fbset -fb /dev/fb0 -xres 240 -yres 320 -vxres 240 -vyres 320

so, I don't know why

dd if=/dev/zero of=/dev/fb0

results in image correct display starting with line 0 on the screen.

I think that writing to framebuffer should fill the complete buffer.

Regards,

Ran

0 Kudos
Reply

2,192 Views
Yuri
NXP Employee
NXP Employee

Hello,

I do not think, that clearing frame buffer fully resolve the issue, if timings are

not correct.


Regards,
Yuri.

0 Kudos
Reply