Hi all,
I am playing maaxboard-mini(i.MX8MM ,yocto sumo, kernel 4.14) with my rtc chip M41T93,
after I set rtc with command: date --set="20210924 20:56:30";hwclock --systohc --utc --rtc=/dev/rtc0 and read it with "hwchock -r" , the date is right. I make sure the rtc works in this kernel
but after reboot, the date and rtc date that reading with hwclock -r both are wrong(it not shows my compilation time, it shows Aug, 26 XXXX)
and I try to use /sbin/hwclock --hctosys to get date, the date are same wrong.
after I remove ntpd.service at /etc/systemd/system/multi-user.target.wants/ntpd.service to disable it
after rebooting and reseting the rtc, and use /sbin/hwclock --hctosys in bootup script, the rtc works well( the date and rtc sync)
it seems ntpd.service make my rtc setting wrong? why? ( I tried yocto zeus, no this issue)
at the first, I think my rtc not work,Maybe the kernel has issue,but I use a scope to check the timing, I find it seems OK. now I think the issue is from ntpd.service
any help?
thanks.
please see the log:
cat /var/log/syslog | grep rtc
Aug 26 14:27:51 fortress kernel: [ 1.713541] imx-drm display-subsystem: bound imx-lcdif-crtc.0 (ops lcdif_crtc_ops)
Aug 26 14:27:51 fortress kernel: [ 4.721802] hctosys: unable to open rtc device (rtc0)
Aug 26 14:27:51 fortress kernel: [ 9.033299] rtc-m41t93 spi0.0: rtc core: registered rtc-m41t93 as rtc0
--
at the first, the log shows :hctosys: unable to open rtc device (rtc0) ,
but finally rtc-m41t93 spi0.0: rtc core: registered rtc-m41t93 as rtc0
the issue is from there?
my yocto sumo and zeus (kernel 4,14 and 5.4) kernel config are same: sync NTP and startup read from rtc
Solved! Go to Solution.
 AldoG
		
			AldoG
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello,
If it still useful for you, it seems that the hwclock and the system clock may not been syncing correctly after reboot, you may try adding the clock synchronization to the startup script, i.e.
hwclock -s
Best regards,
Aldo.
 AldoG
		
			AldoG
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello,
If it still useful for you, it seems that the hwclock and the system clock may not been syncing correctly after reboot, you may try adding the clock synchronization to the startup script, i.e.
hwclock -s
Best regards,
Aldo.
Hi @AldoG
it's useful.
I did the same with :/sbin/hwclock --hctosys it's well
Thank you very much.
I received your answer as an solution