it have a error when use uuu toools download program to imx8qm

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

it have a error when use uuu toools download program to imx8qm

3,766 Views
zhaowei49
Contributor I

SOC : IMX8QM ; 

Flash : mircron emmc 64G(MTFC64GAPALBH-AIT)

Description :  Six new boards need checked hardware function . The one of sixes had a failture as below but others were ok.  when  download  program to flash with uuu tool by usb port , and process run to step 14 ,it stopped and displayed a hint "no flash device defined " . The attached the picture 1 is  program lists that need downloading.The attached the picture 2 is  hint cam shooting.

0 Kudos
Reply
1 Reply

3,756 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Zhaowei,

The following suggestions are for your reference:
1. Use uuu -b emmc u-boot.imx (here should be your bootloader's name) to flash the bootloader, other images are not downloaded to the board.
2. Boot board
Power off the board and configure it to boot from eMMC to check whether it can boot normally.
3. If the above method fails to start the board or the download is abnormal, then find the problem on the hardware. Mainly find the problem on SMT.

-------------

以下建议供您参考:
1. 使用uuu -b emmc u-boot.imx( here should be your bootloader's name)命里烧写bootloader,其他的image不是下载到板子。
2. boot板子
给板子断电,并配置为从eMMC启动,检查是否可以正常启动。
3. 如果上述方法,无法启动板子或者下载不正常,那么要在硬件上查找问题。主要在SMT上查找问题。

-------------------------

 

Have a nice day!

B.R,

Weidong

0 Kudos
Reply