issue : eth0 can not ping DUT. Please help !!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

issue : eth0 can not ping DUT. Please help !!

3,953 次查看
jason9tsai
Contributor I

I try to ping DUT in the same domain, but it can not work.

SoC I.MX6 

Module RTL8201F 

  • I have check eth0, and modify IP addr.

$/etc/init.d/networking stop

$ifconfig eth0 hw ether 82:1d:e5:23:53:15

$/etc/init.d/networking start

$ifconfig eth0 192.168.1.4 up

$ ifconfig

ifconfig.png

  • I have used ethtool to check. And I  remove Network Cable , the log has show link is not ready .pastedImage_1.png
  • I have check dmesg. It looks okay.

Log is show :

Line 142: [ 1.165081] fec 20b4000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00
Line 143: [ 1.173870] fec 20b4000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: 82:1d:e5:23:53:15
Line 144: [ 1.183851] libphy: fec_enet_mii_bus: probed
Line 145: [ 1.189958] fec 20b4000.ethernet eth0: registered PHC device 0
Line 148: [ 1.206324] fec 2188000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00
Line 149: [ 1.215269] fec 2188000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: 96:a6:86:e0:fa:d7
Line 150: [ 1.226631] fec 2188000.ethernet eth1: registered PHC device 1
Line 430: [ 8.081647] fec 20b4000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=20b4000.ethernet:01, irq=-1)
Line 430: [ 8.081647] fec 20b4000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=20b4000.ethernet:01, irq=-1)
Line 432: [ 9.331924] fec 20b4000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=20b4000.ethernet:01, irq=-1)
Line 432: [ 9.331924] fec 20b4000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=20b4000.ethernet:01, irq=-1)
Line 453: [ 12.341901] fec 20b4000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
Line 457: [ 191.521890] fec 20b4000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=20b4000.ethernet:01, irq=-1)
Line 457: [ 191.521890] fec 20b4000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=20b4000.ethernet:01, irq=-1)
Line 458: [ 193.522608] fec 20b4000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx

 

  • The phy_id is show 0x001cc816. It is for RTL8201F.

phy_id.png

 

0 项奖励
回复
3 回复数

2,950 次查看
igorpadykov
NXP Employee
NXP Employee

Hi jason

had you used linux driver for that chip:

net: phy: realtek: add rtl8201f driver - Patchwork 

first please try in uboot, seems processor used in that case is i.MX6UL, try nxp uboot:

http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/?h=imx_v2016.03_4.1.15_2.0.0_ga

also one can try loopback test.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,950 次查看
jason9tsai
Contributor I

Hello Igor,

   I have modify device-tree, it can work.

   Thanks for you help !!

&fec1 {
   pinctrl-names = "default";
   pinctrl-0 = <&pinctrl_enet1>;
   phy-mode = "rmii";
   status = "okay";

};

pinctrl_enet1: enet1grp {
   fsl,pins = <
      MX6UL_PAD_GPIO1_IO07__ENET1_MDC 0x1b0b0
      MX6UL_PAD_GPIO1_IO06__ENET1_MDIO 0x1b0b0
      MX6UL_PAD_ENET1_RX_EN__ENET1_RX_EN 0x1b0b0
      MX6UL_PAD_ENET1_RX_ER__ENET1_RX_ER 0x1b0b0
      MX6UL_PAD_ENET1_RX_DATA0__ENET1_RDATA00 0x1b0b0
      MX6UL_PAD_ENET1_RX_DATA1__ENET1_RDATA01 0x1b0b0
      MX6UL_PAD_ENET1_TX_EN__ENET1_TX_EN 0x1b0b0
      MX6UL_PAD_ENET1_TX_DATA0__ENET1_TDATA00 0x1b0b0
      MX6UL_PAD_ENET1_TX_DATA1__ENET1_TDATA01 0x1b0b0
      MX6UL_PAD_ENET1_TX_CLK__ENET1_REF_CLK1 0x4001b031
   >;
};

Best regards
Jason

0 项奖励
回复

2,950 次查看
jason9tsai
Contributor I

any one can help me ?

0 项奖励
回复