iperf-1.7.0-vork.path missing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iperf-1.7.0-vork.path missing

3,443 Views
Swamy
Contributor III

Hello,

I am trying to build for IMX53QSB using LTIB. I am getting following error. I am not able to find this package for download. please suggest how to resolve this issue.

 

Regards,

Swamy

 

Processing: iperf
===================
Build path taken because: no prebuilt rpm,
Testing network connectivity
No network download connection available

Can't get: iperf-1.7.0-vfork.patch at ./ltib line 790.


f_buildrpms() returned an error, exiting

Labels (1)
0 Kudos
Reply
4 Replies

3,061 Views
mohammedzakariy
Contributor I

Hi Swamy,

Did you got solution for iperf-1.7.0-vfork.patch issue, i am facing same problem for building i.MX35.

Can you provide some details if you have.

Thanks,

Mohammed zakariya

0 Kudos
Reply

3,061 Views
SreekumarRG
Contributor I

Hi All,

  Can any one help me to find the performance of ethernet using iperf in imx processor,

  As iam the hardwrae guy not much more about the software side , please try to give right path from the bottom end.

 

Thanks in advance,

Sree

0 Kudos
Reply

3,061 Views
daiane_angolini
NXP Employee
NXP Employee

Are you sure you have all needed package to LTIB install?

 

Please, take a look here http://www.imxdev.org/wiki/index.php?title=All_Boards_LTIB in order to double check.

0 Kudos
Reply

3,061 Views
MaciejHalasz
Contributor I

Hi,

 

Don't know if it will interest you but you can build a custom free BSP for i.MX53QSB entirely online at:

 

linuxlink.timesys.com

 

After the build is done you can download both BSP and SDK as customized for your needs.

The Linux kernel available there is the same as in FSL enablement code (LTIB) but all the userspace packages are recent version. There are over 1000 APIs to choose from. The iperf version available is 2.0.4.

 

HTH

Maciej

0 Kudos
Reply