interfacing 32 bit GPIF II with 32 bit EIM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

interfacing 32 bit GPIF II with 32 bit EIM

1,711 Views
nanthanraj
Contributor I

Hi,

what is the possibility and challenges for interfacing i.MX7solo EIM port with EZ-USB FX3 GPIF II in 32 bit mode?

what is the possible data bandwidth can be achieved?

Regards,

Nanthan.

Labels (1)
0 Kudos
Reply
1 Reply

1,599 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nathan

there are no problems with connection any devices with parallel nor - like interface,

for performance estimations please look at

https://community.freescale.com/docs/DOC-106467

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply