install sdk error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

install sdk error

1,793件の閲覧回数
llr
Contributor I

Hello,

      I successfully compiled the SDK using the following command.

      repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-zeus -m imx-5.4.70-2.3.0.xml

      DISTRO=fsl-imx-wayland MACHINE=imx8mmevk source imx-setup-release.sh -b build-wayland
      bitbake imx-image-full -c populate_sdk

      However, an error occurred when installing the SDK. How should I solve this problem?

      HOST: ubuntu 16.04QQ图片20210223181156.png

0 件の賞賛
返信
2 返答(返信)

1,784件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi llr

 

one can follow sect.3 Host Setup i.MX Yocto Project User’s Guide​

"The recommended minimum Ubuntu version is 18.04 or later."

 

Best regards
igor

0 件の賞賛
返信

1,779件の閲覧回数
llr
Contributor I

I tried installing the SDK in Ubuntu 18.04 and got the same error.

I built the SDK in Ubuntu 16.04. Do I have to recompile the SDK in Ubuntu 18.04?

0 件の賞賛
返信