inflexion ui plugin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

inflexion ui plugin

1,615件の閲覧回数
Lyven
Contributor II

Hello all

I try to load the plugin from the demo into my own inflexion ui appliciaton. I add a plugin to my root.template. I refer through Resource->event handler = "demoPluginElement://" to my  ifxui_plugin.plugin file. In the editor the sinewave.png is visible (so I think the reference is good). However when i start up my application on the imx53 QSB, nothing appears. I just the exact same module code from the example and I made the integration layer with my UIintegrator.exe. 

I think it has something to do with the startup of the element itself. (Since I checked which functions works with printf()). So I added a touchregion which tried to start the element. which got the IFX_RETURN_STATUS IFXM_ifxuiplugin_ExecuteLink_ButtonLink() function working but still nothing to see on the screen.

Anyone has an idea?

thanks in advance

kind regards

Lieven

タグ(1)
0 件の賞賛
返信
1 返信

1,571件の閲覧回数
PhilBrumby
Fresh Out Contributor

This query is currently being dealt with in the InflexionUI Community.

http://communities.mentor.com/mgcx/message/27682#27682

Phil.

0 件の賞賛
返信