imxrt1061 vs 1062 vs 106[AFLS]

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imxrt1061 vs 1062 vs 106[AFLS]

904 Views
bennxp
Contributor III

I have a design that uses the MIMXRT1062 but given challenges in part availability, I'm wondering if there are drop-in equivalent parts. Looking at https://www.nxp.com/docs/en/nxp/data-sheets/IMXRT1060CEC.pdf I can't understand the difference between the 1061 and 1062. The "Part number nomenclature" states the that 1061 is the "standard feature" version and the 1062 is the "full feature" version, but features listed in the table 1 are the same for both chips. Is there a document that lists what is different between the two chips?

Also, there a few special purpose chips  (106A, 106F, 106L, 106S) that also have the same feature list. Could this be drop-in replacements for the 1062? Is there a document explaining what is different with these chips?

Thanks,

 

0 Kudos
Reply
0 Replies