imx95 npu support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx95 npu support

2,618 Views
nigelzzz
Contributor I

Hi,
   We are using imx95 develop some machine learning app. so I need some sample code and doc to check npu performance and learn how to use the npu to calculate complex operation.

first question: 
I reference the document from nxp, it says we can use "label_image" to check the performance on npu and cpu.

-  npu version: ./label_image -m mobilenet_v1_1.0_224_quant.tflite -i grace_hopper.bmp -l labels.txt --external_delegate_path=/usr/lib/libneutron_delegate.so

- cpu version: ./label_image -m mobilenet_v1_1.0_224_quant.tflite -i grace_hopper.bmp -l labels.txt .

the average time always return 16.xxx ms, why it doesn't improve when i using npu.

INFO: Loaded model mobilenet_v1_1.0_224_quant.tflite
INFO: resolved reporter
INFO: invoked
INFO: average time: 16.558 ms
INFO: 0.764706: 653 military uniform
INFO: 0.121569: 907 Windsor tie
INFO: 0.0156863: 458 bow tie
INFO: 0.0117647: 466 bulletproof vest
INFO: 0.00784314: 835 suit

 

the second question is i see /usr/lib/libneutron_delegate.so can load "NeutronKernels.bin and NeutronFirmware.elf", can we get the source code?

reference document
- https://www.nxp.com/docs/en/user-guide/IMX-MACHINE-LEARNING-UG.pdf
- https://github.com/nxp-imx/neutron

- https://github.com/nxp-imx/tflite-neutron-delegate

Tags (1)
0 Kudos
Reply
2 Replies

2,595 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @nigelzzz!
Thank you for contacting NXP Support!

Sorry, we can´t provide the source code of those binaries.

The iMX95 is not available for all.

To get support I recommend to ask directly to your local DFAE.

Sorry for the mistake!

Best Regards!
Chavira

0 Kudos
Reply

2,582 Views
nigelzzz
Contributor I

Hi,

   Do you have any suggestion on how to check the npu on imx95 is work.
I see we can use label_image to check performance on npu/gpu/cpu.

Does the imx95 have similiar tool to check?

0 Kudos
Reply