imx95 19x19 board using codec as master example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx95 19x19 board using codec as master example

Jump to solution
1,432 Views
andyhuang_msi
Contributor III

Hi everyone:

Our project using TI's codec 6PAIC3104IRHBRQ1.

BCLK, WCLK, DIN and DOUT are connected to SAI3 module of soc.

But the MCLK is connected to external Oscillator, OSC-24MHZ30_S-HF instead of SAI3 module of soc.

In this condition, the master CLK is provided by codec not by SAI3 module of soc.

I would like to ask if anyone could provide dts example of master CLK provided by codec. 

If necessary, I could provide my patch for review.

 

 

0 Kudos
Reply
1 Solution
1,067 Views
andyhuang_msi
Contributor III

The HW has modified to MCLK connected to soc instead of external oscillator.

After adjusting setting of tinymix, the speaker is capable of audio output.

This issue should be closed.

View solution in original post

0 Kudos
Reply
5 Replies
1,406 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Unfortunately this CODEC is not supported by default on our BSP and there is no a guide to port it. The references we have are the i.MX porting guide.

My recommendation is declare the fixed clock configuration in CODEC side as follows:

codec_mclk: codec_mclk {
        compatible = "fixed-clock";
        #clock-cells = <0>;
        clock-frequency = <24000000>;
};

And use this properties to configure you CODEC as master, for example:

simple-audio-card,bitclock-master = <&dailink_codec>;
simple-audio-card,frame-master = <&dailink_codec>;

Best regards.

0 Kudos
Reply
1,388 Views
andyhuang_msi
Contributor III

@JorgeCas 

Thanks for your reply.

I found the codec driver of TI audio codec on imx95  bsp: 

vendor/nxp-opensource/kernel_imx/sound/soc/codecs/tlv320aic3x.c

vendor/nxp-opensource/kernel_imx/sound/soc/codecs/tlv320aic3x-i2c.c

 

I modify defconfig file(arch/arm64/configs/imx95_gki.fragment) to add two drivers into compile:

+CONFIG_SND_SOC_TLV320AIC3X=m
+CONFIG_SND_SOC_TLV320AIC3X_I2C=m      

device/nxp/imx9/evk_95/SharedBoardConfig.mk

BOARD_VENDOR_KERNEL_MODULES += \

+ $(KERNEL_OUT)/sound/soc/codecs/snd-soc-tlv320aic3x.ko \
+ $(KERNEL_OUT)/sound/soc/codecs/snd-soc-tlv320aic3x-i2c.ko \

 

I also take your suggestion and modify dts.

The attached files containing modified dts, imx95-19x19-evk.dts and patch, imx95_evk_dts.patch.

The following section details the changes and their purposes.

(1)&sai3, pinctrl_sai3, pinctrl_sai3_sleep:

      BCLK, WCLK, DIN and DOUT gpio of audio codec connect to SAI3 module of soc.

      MCLK gpio not connected to soc and comment.

(2)codec_mclk: codec-mclk

 add a fixed clock as suggestion

(3)tlv320aic3x: tlv320aic3x@18

audio codec driver node

clocks = <&codec_mclk>;   reference to fixed clock codec_mclk

(4)sound-tlv320aic3x

dai connection of sai3 module of soc and TI audio codec

 simple-audio-card,bitclock-master and simple-audio-card,frame-master reference dailink_master_codec as master.

The dailink_master_codec set clocks to fixed clock codec_mclk。

 

I prepare three audio wav files and use tinyplay to test speaker of audio codec.

Although no error messages happened during test prieod of the three wav files, I cannot hear the audio.

ex:

tinyplay /sdcard/rhj08-s3gh1_2.wav -D 2

Playing sample: 2ch, 48000 hz, 16bit 1414376 bytes
Draining... Wait 85333 us

 

I also use some commands, i2cdetect, lsmod, cat /proc/asound/cards , tinypcminfo -D 2, cat /sys/kernel/debug/clk/clk_summary | grep "codec-mclk" and tinyplay command to test the audio codec.

The results are listed in the attached file, audio_test_commands_results.txt.

 

I would like to ask if  any suggestion about current dts or linux command to check status of audio codec?

 

 

 

 

0 Kudos
Reply
1,364 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Thank you for the update.

Please try to change the clock configuration as is in commented SAI3 node:

assigned-clock-rates = <3932160000>,
    <3612672000>, <393216000>,
    <361267200>, <12288000>;

If possible please confirm if there are activity in SAI signals when sound should be playing.

Also, I suggest you confirm if the audio routing is according to the outputs you are using.

Could you please share your dmesg?

Best regards.

0 Kudos
Reply
1,303 Views
andyhuang_msi
Contributor III

 

@JorgeCas 

Thanks for your reply.

Considering HW change doubt, we have changed MCLK of HW design connecting to GPIO17 of soc instead of external oscillator.

I also modify dts corresponding to HW change and not hear audio sound using tinyplay command to play 48000 rate wav file.

 

Our EE measure the activity in SAI3 signals:

SAI3_TX_BCLK,SAI3_TX_SYNC, SAI3_TX_DATA_BIT0, SAI3_MCLK all detect signal TX and CODEC_SAI3_RXD not detect signal TX.
And the LEFT_LOP and LEFT_LOM of audio codec connected to speaker amplifier not detect signal TX.
 
 
The attached zip file contain whole dts file: imx95-19x19-evk.dts
                                                    dts file patch: 0608_evk_dts_audio.patch
                                                    dmesg file       :teraterm_0608_dmesg  
                                                    command test result file: audio_commands_results_0608.txt
                                                    current audio codec driver: tlv320aic3x.c, tlv320aic3x-i2c.c
 
The audio routing is according to the driver, tlv320aic3x.c  part: 
static const struct snd_soc_dapm_route intercon[]
/* Left Line Output */  and   /* Right Line Output */
 
 
I use some commands to check status of audio codec:
cat /sys/kernel/debug/clk/clk_summary | grep -A5 -B5 sai3
before tinyplay wav file:

sai3                          0       0        0        12288000    0          0     50000      Y         tlv320aic3x@18                  no_connection_id

                                                                                                                                     42650000.sai                       mclk1

during tinyplay wav file:

sai3                          1       1        0        12288000    0          0     50000      Y         tlv320aic3x@18                  no_connection_id

                                                                                                                                     42650000.sai                      mclk1

->enable_cnt  and prepare_cnt of sai3 has changed.

 
 
Question1:
Does my dts modified has any wrong setting?
Question2:
How do I check if the setting of audio routing part is correct?
0 Kudos
Reply
1,068 Views
andyhuang_msi
Contributor III

The HW has modified to MCLK connected to soc instead of external oscillator.

After adjusting setting of tinymix, the speaker is capable of audio output.

This issue should be closed.

0 Kudos
Reply