imx93 spi3 testing.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx93 spi3 testing.

2,424件の閲覧回数
sbmd_1234
Contributor III

Hi NXP team,

I have created the node and pin settings for the spi3 in dts but I am unable the see the spidev_test data tx/rx as shown in the logs  I have connected the MOSI and MISO pins also for loopback but no rx data I am getting pls check : 

dts : 

&lpspi3 {
#address-cells = <1>;
#size-cells = <0>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_lpspi3>;
cs-gpios = <&gpio2 8 GPIO_ACTIVE_LOW>;
fsl,spi-num-chipselects = <1>;
status = "okay";

spidev0: spi@0 {
compatible = "rohm,dh2228fv";
spi-max-frequency = <1000000>;
reg = <0>; /* Chip select 0 */
};
};


pinctrl_lpspi3: lpspi3grp {
fsl,pins = <
MX93_PAD_GPIO_IO08__LPSPI3_PCS0 0x3fe
MX93_PAD_GPIO_IO08__GPIO2_IO8 0x3fe
MX93_PAD_GPIO_IO09__LPSPI3_SIN 0x3fe
MX93_PAD_GPIO_IO10__LPSPI3_SOUT 0x3fe
MX93_PAD_GPIO_IO11__LPSPI3_SCK 0x3fe
>;
};



spidev_test logs : 

spidev_test -D /dev/spidev0.0 -v -p "hello"
spi mode: 0x0
bits per word: 8
max speed: 500000 Hz (500 kHz)
TX | 68 65 6C 6C 6F __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ |hello|
RX | FF FF FF FF FF __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ |.....|


spidev_test -D /dev/spidev0.0 -v
spi mode: 0x0
bits per word: 8
max speed: 500000 Hz (500 kHz)
TX | FF FF FF FF FF FF 40 00 00 00 00 95 FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF F0 0D |......@.........................|
RX | FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF |................................|


please help me to resolve this.

thanks.

0 件の賞賛
返信
4 返答(返信)

2,393件の閲覧回数
sbmd_1234
Contributor III

Hi,

Any suggestions on this I want to validate the spi interface please help in this.


Thanks.

0 件の賞賛
返信

2,367件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @sbmd_1234 

 

I hope you are doing very well.

 

Please refer to the imx93-11x11-evk-lpspi.dts.

Then, you should be able to get it working:

Without connection between SIN and SOUT:

Alejandro_Salas_0-1729533982466.png

 

With connection between SIN and SOUT:

Alejandro_Salas_1-1729534016576.png

Alejandro_Salas_2-1729534043249.png

 

FYI: tested on imx93evk and 6.6.23 bsp

Alejandro_Salas_3-1729534076938.png

 

Best regards,

Salas.

 

 

0 件の賞賛
返信

2,345件の閲覧回数
sbmd_1234
Contributor III

HI @Manuel_Salas 

Thanks for your support!

Do I need to add the lpspi3 node in imx93-11x11-evk.dts file, or can we work with the DTS files "imx93-11x11-evk-lpspi.dts and imx93-11x11-evk-lpspi-slave.dts" as the spi configuration is already done?

Also, I cannot see the /dev/spidev interface if I am not adding the node in  imx93-11x11-evk.dts file. Please help in this what configurations actually I need to validate the spi.


Thanks.

0 件の賞賛
返信

2,328件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @sbmd_1234 

You can use imx93-11x11-evk-lpspi.dts directly and then you will be able to use the lpspi interface.

 

Best regards,

Salas.

0 件の賞賛
返信