imx8qxp eMMC boot issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8qxp eMMC boot issue

3,951 Views
zhengguang_yang
Contributor II

Hi 

I'm using imx8qxp, Yocto 3.0.

The same image boot normally on the SD card, but after burning to EMMC, there is no log output in the uboot phase, and the kernel phase is normal.

I feel this phenomenon is so strange and I don't have any ideas, so I'd like to ask if you have any good ideas

 

0 Kudos
Reply
7 Replies

3,947 Views
jimmychan
NXP TechSupport
NXP TechSupport

Which board are you using?

Do you change the boot mode to boot from the EMMC?

0 Kudos
Reply

3,945 Views
zhengguang_yang
Contributor II

Hi Jimmychan:

Thank you for your reply.

We use our customized board.

Boot mode has been modified to boot from EMMC.

 

0 Kudos
Reply

3,939 Views
jimmychan
NXP TechSupport
NXP TechSupport

After you boot up from the SD card, can you mount the EMMC in Linux? Do you see any content in the EMMC?

0 Kudos
Reply

3,933 Views
zhengguang_yang
Contributor II

After starting from the SD card, we can successfully mount the EMMC, and the same content as the SD card can be seen in the EMMC.

Unplug the SD card, the EMMC boot normally, but there is no log output in the uboot phase.

0 Kudos
Reply

3,930 Views
jimmychan
NXP TechSupport
NXP TechSupport

"EMMC boot normally, but there is no log output in the uboot phase".

Sorry, what does it means? do you mean the board can normal boot up but no console output from debug uart? 

0 Kudos
Reply

3,925 Views
zhengguang_yang
Contributor II

Yes, there is no log output in the uboot phase, and the kernel phase is normal.

0 Kudos
Reply

3,919 Views
jimmychan
NXP TechSupport
NXP TechSupport

Have you try to program the u-boot (in your SD card) to the EMMC?

0 Kudos
Reply