imx8qxp eMMC boot issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8qxp eMMC boot issue

3,794件の閲覧回数
zhengguang_yang
Contributor II

Hi 

I'm using imx8qxp, Yocto 3.0.

The same image boot normally on the SD card, but after burning to EMMC, there is no log output in the uboot phase, and the kernel phase is normal.

I feel this phenomenon is so strange and I don't have any ideas, so I'd like to ask if you have any good ideas

 

0 件の賞賛
返信
7 返答(返信)

3,790件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Which board are you using?

Do you change the boot mode to boot from the EMMC?

0 件の賞賛
返信

3,788件の閲覧回数
zhengguang_yang
Contributor II

Hi Jimmychan:

Thank you for your reply.

We use our customized board.

Boot mode has been modified to boot from EMMC.

 

0 件の賞賛
返信

3,782件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

After you boot up from the SD card, can you mount the EMMC in Linux? Do you see any content in the EMMC?

0 件の賞賛
返信

3,776件の閲覧回数
zhengguang_yang
Contributor II

After starting from the SD card, we can successfully mount the EMMC, and the same content as the SD card can be seen in the EMMC.

Unplug the SD card, the EMMC boot normally, but there is no log output in the uboot phase.

0 件の賞賛
返信

3,773件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

"EMMC boot normally, but there is no log output in the uboot phase".

Sorry, what does it means? do you mean the board can normal boot up but no console output from debug uart? 

0 件の賞賛
返信

3,768件の閲覧回数
zhengguang_yang
Contributor II

Yes, there is no log output in the uboot phase, and the kernel phase is normal.

0 件の賞賛
返信

3,762件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Have you try to program the u-boot (in your SD card) to the EMMC?

0 件の賞賛
返信