Hi!
After flashing imx8qmmek board with Zeus image built from manifest imx-5.4.70-2.3.1.xml:
uuu -b emmc_all imx-boot core-image-minimal-imx8qmmek.wic.bz2
Loading a Zeus image, through tftpboot (kernel and dtb), works fine.
But loading a Sumo image, through tftpboot (kernel and dtb), leads to :
mmc0: Timeout waiting for hardware interrupt.
[ 44.267871] mmc0: sdhci: ============ SDHCI REGISTER DUMP ===========
[ 44.274315] mmc0: sdhci: Sys addr: 0x00000000 | Version: 0x00000002
[ 44.280761] mmc0: sdhci: Blk size: 0x00000200 | Blk cnt: 0x00000001
[ 44.287206] mmc0: sdhci: Argument: 0x00000000 | Trn mode: 0x00000013
[ 44.293644] mmc0: sdhci: Present: 0x01fd8a0a | Host ctl: 0x00000011
[ 44.300083] mmc0: sdhci: Power: 0x00000002 | Blk gap: 0x00000080
[ 44.306518] mmc0: sdhci: Wake-up: 0x00000008 | Clock: 0x000080ff
[ 44.312956] mmc0: sdhci: Timeout: 0x0000008f | Int stat: 0x00000000
[ 44.319393] mmc0: sdhci: Int enab: 0x107f100b | Sig enab: 0x107f100b
[ 44.325831] mmc0: sdhci: AC12 err: 0x00000000 | Slot int: 0x00000502
[ 44.332271] mmc0: sdhci: Caps: 0x07eb0000 | Caps_1: 0x8000b407
[ 44.338714] mmc0: sdhci: Cmd: 0x0000083a | Max curr: 0x00ffffff
[ 44.345152] mmc0: sdhci: Resp[0]: 0x00000900 | Resp[1]: 0xffffffff
[ 44.351589] mmc0: sdhci: Resp[2]: 0x320f5903 | Resp[3]: 0x00d07f01
[ 44.358026] mmc0: sdhci: Host ctl2: 0x00000000
[ 44.362466] mmc0: sdhci: ADMA Err: 0x00000009 | ADMA Ptr: 0xfffff200
[ 44.368902] mmc0: sdhci: ============================================
[ 44.375451] mmc0: error -110 whilst initialising MMC card
The same procedure, but on a board flashed with Sumo image, used to work fine.
Could it be a uboot/kernel Zeus/Sumo incompatibility?
Thanks!
Solved! Go to Solution.
Hi fabatera
>Could it be a uboot/kernel Zeus/Sumo incompatibility?
in general yes, as each uboot/linux versions should be formally aligned as
described in Release Notes document on linux documentation link
Also it is necessary to follow sect.1.2 System Controller Firmware (SCFW) Requirements
i.MX 8QuadMax Automotive and Infotainment Applications Processors
Best regards
igor
Hi fabatera
>Could it be a uboot/kernel Zeus/Sumo incompatibility?
in general yes, as each uboot/linux versions should be formally aligned as
described in Release Notes document on linux documentation link
Also it is necessary to follow sect.1.2 System Controller Firmware (SCFW) Requirements
i.MX 8QuadMax Automotive and Infotainment Applications Processors
Best regards
igor