大家好:
我现在使用的是imx8qm mek 板子,当前的android P9 AUTO 版本只能编译出lvds-hdmi显示的版本,请问现在 android P9 AUTO版本代码已经支持板载的HDMI_TX显示吗?如果有,需要怎么配置?谢谢~
hi everyone:
I am using the imx8qm mek board now, the current android P9 AUTO version can only compile the version shown by lvds-hdmi, may I ask whether the code of android P9 AUTO version already supports the display of HDMI_TX on the board?If yes, how do I configure it?thank you~
Hello Yuelin,
i.MX8QM is still in pre-production now, I can only give you some guidance on your questions. see below, please!
---------------------
You will need to re-compile device tree with fsl-imx8qm-mek-hdmi.dts, then check if hdmi driver has been selected in linux kernel, if not, select it , please! then re-compile kernel, and try.
--------------------
Hope above information can help you!
Have a nice day!
BR,
Weidong