imx8qm: SSD not detected

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8qm: SSD not detected

817件の閲覧回数
GauravSinha
Contributor I

Reference Board : i.MX8QMax

Issue : SSD not detected with newer SD card Images available on the download page

Description :

I have tried the below S/W versions and flashed the image to sd card using the command "sudo dd if=<image name>.wic of=/dev/mmcblkX bs=1M && sync"

  • LF_v5.10.72-2.2.0_images_IMX8QMMEK
  • L5.4.70-2.3.0_images_MX8QMMEK

The detection of SSD is no more consistent & fails with different reasons.. On 4.14 kernel, the SSD is consistently detected fine.

Different errors are reported below:

LF_v5.10.72-2.2.0_images_IMX8QMMEK

-----------------------------FAIL CASE--------------------------------------------------

[ 3.835709] imx6q-pcie 5f010000.pcie: Phy link never came up
[ 3.857896] imx6q-pcie 5f010000.pcie: failed to initialize host
[ 3.863846] imx6q-pcie 5f010000.pcie: unable to add pcie port.

--------------------------------------------------------------------------------

---------------------------------PASS CASE-----------------------------------------------

[ 3.162121] pci 0000:01:00.0: reg 0x10: [mem 0x00000000-0x00003fff 64bit]
[ 3.176317] pci 0000:01:00.0: 7.876 Gb/s available PCIe bandwidth, limited by 8 GT/s x1 link at 0000:00:00.0 (capable of 31.504 Gb/s with 8 GT/s x4 link)

--------------------------------------------------------------------------------

 

LF_v5.10.72-2.2.0_images_IMX8QMMEK

--------------------------------------------------------------------------------------------

[ 3.628753] nvme 0000:01:00.0: of_irq_parse_pci: failed with rc=134
[ 3.629054] nvme nvme0: pci function 0000:01:00.0
[ 3.743731] nvme 0000:01:00.0: enabling device (0000 -> 0002)
[ 3.750826] nvme nvme0: Removing after probe failure status: -19

--------------------------------------------------------------------------------------------

 

ラベル(1)
0 件の賞賛
返信
1 返信

799件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @GauravSinha 

Can you share specific model of your SSD?

 

Best Regards

Zhiming

0 件の賞賛
返信