How to route an external MCLK to multiple SAIs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to route an external MCLK to multiple SAIs

2,037件の閲覧回数
wsl0824
Contributor I

 

[ Setup ]

 
[ Background ] 
The objective is to synchronously render the audio signals received from a wireless IC (stereo in I2S format) through the WM8524 codec available on the iMX8MM EVK. Since the wireless IC relays the host audio timing, the SAI MCLKs on iMX8MM should be in sync with the MCLK coming from the wireless IC. The following depicts the system configuration and the two possible options for the MCLK routing. Based on the figures below, the goal is to use MCLK_5 as the MCLK for all the SAIs operating inside the iMX8MM.
 

1) Receive the external MCLK via SAIn_MCLK input pad

wsl0824_0-1639768619788.png

According to the iMX8MM reference manual, it is possible for both SAI5 and SAI3 to use the MCLK_5 as the master clock if MCLK_5 is fed to the SAI5_MCLK pad and the IOMUXC_GPR registers are configured accordingly. However, I don't see any document/examples about how to configure it correctly. I took a look at the Linux source files (e.g., fsl_sai.c, fsl_sai_sysfs.c), but it seems like such control is not implemented anywhere. 

2) Receive the external MCLK via EXT_CLKn pin

wsl0824_0-1639771278270.png

Another possibility is to receive the MCLK_5 via EXT_CLK2 pin and distribute internally through the clock tree. But, the EXT_CLK2 pin is not readily accessible on the iMX8MM EVK. Also, it is less preferreable than the prior method of using the IOMUXC_GPR registers becuase we plan to involve additional SAI for our end appliaction. While the EXT_CLKn is shared between subset of SAIs, the IOMUXC_GPR-based method allows a complete flexibility in choosing the MCLK source. 

[ Questions ]

Q1. So far, I was able to customize the kernel using 'simple-audio-card' to record (i.e., arecord) the audio stream coming from the wireless IC. However, I used the IMX8MM_AUDIO_PLL1_OUT as the MCLK. How can I use the MCLK_5 on SAI5_MCLK pad as the master clock? (FYI, the following is my device tree snippet). 

 

 

/dts-v1/;
#include "imx8mm-evk.dts"
/ {
    // wac: wireless audio codec
	wac: wac {
		#sound-dai-cells = <0>;
		compatible = "test,wac";
		status = "okay";
	};

	sound-wac {
		compatible = "simple-audio-card";
		simple-audio-card,name = "wac";

		simple-audio-card,dai-link@0 {
			format = "i2s";
			bitclock-master = <&wac_dai>;
			frame-master = <&wac_dai>;

			wac_cpu: cpu {
				sound-dai = <&sai5>;
			};

			wac_dai: codec {
				sound-dai = <&wac>;
			};
		};
	};
};

&sai5 {
	#sound-dai-cells = <0>;
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_sai5>;
	assigned-clocks = <&clk IMX8MM_CLK_SAI5>;
	assigned-clock-parents = <&clk IMX8MM_AUDIO_PLL1_OUT>;
	assigned-clock-rates = <1536000>;    
	status = "okay";
};

&iomuxc {
	pinctrl_sai5: sai5grp {
		fsl,pins = <
			MX8MM_IOMUXC_SAI5_MCLK_SAI5_MCLK        0xd6
			MX8MM_IOMUXC_SAI5_RXC_SAI5_RX_BCLK      0xd6
			MX8MM_IOMUXC_SAI5_RXFS_SAI5_RX_SYNC     0xd6
			MX8MM_IOMUXC_SAI5_RXD0_SAI5_RX_DATA0    0xd6
		>;
	};
};

 

 

Q2. Once the Question 1 has been addressed, how and where can I configure the IOMUXC_GPR registers to use SAI5_MCLK (i.e., MCLK_5) as the master clock for the SAI3?

Q3. In another thread, it says that the system hangs during the boot if a clock is not present on EXT_CLKn pin. Is it the expected behavior? In other words, should the MCLK_5 be available before the system boot and be always present?

Q4. I wonder if the same or similar issue as Q3 is also present in the case of using the SAIn_MCLK pad to feed the external clock. Does MCLK_5 have to be present all the time before the system boot and while the system is operating? 

Q5. Continued from Q4, what happens if we activate SAI3 (e.g., aplay) while MCLK_5 is not present? 

Thanks,

Woosuk

 

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

2,009件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

@wsl0824 

For Q2:you should use

MX8MM_IOMUXC_SAI3_MCLK_SAI5_MCLK

, this config will let SAI3_MCLK select SAI5_MCLK as an input source.

 

For Q3 and Q4 ,I need some time to find if that patch has been merged to our latest BSP.

0 件の賞賛
返信

1,984件の閲覧回数
wsl0824
Contributor I

 

@Zhiming_Liu Thanks for the reply. 

Q1) I confirmed that the wireless audio receiver outputs the MCLK_5 before getting connected to the iMX8MM EVK. But it disappears after connected to the EVK. It seams that the SAI5_MCLK pad is set to an output probably because the clock setting in my device tree was incorrect. Although SAI5 is working well as a slave without the MCLK_5, it is important to receive MCLK_5 so that it can be routed to MCLK_3 output.

  • Could you please share an example how to properly configure the device tree to receive an external MCLK to SAI5?

 

Q2) I tried your suggestion, but no luck. Page 3896 of the iMX8MM RM says that the IOMUX_GPR registers have to be configured to use alternative MCLK options.

  • By specifying below, does it take care of the IOMUX_GPR settings as well? Which function/source file should I look at to observe the configuration process?
MX8MM_IOMUXC_SAI3_MCLK_SAI5_MCLK
  • Could you please share a device tree snippet showing how to route MCLK_5 input to MCLK_3 output?

 

Q3/Q4)

  • Do you have any update on this?
  • Could you please share a link to the patch details?
0 件の賞賛
返信

1,931件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Q1: According to RM, bit clock can be set as externally generated. Can you set it manually with memtool? The register address is 30050090 for SAI5 RCR2, Bit Clock Direction, you can see the explanation for MCLK Select.

Q2:MX8MM_IOMUXC_SAI3_MCLK_SAI5_MCLK mux sai3_mclk pad as sai5_mclk , the sai3_mclk is sai5_mclk.

0 件の賞賛
返信