imx8mp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mp

851 Views
qwerqq
Contributor I

Hello:

Hello:

My network port hardware is set to 1000Mb/s, and the phy is also 1000Mb/s phy. My switch has two modes, one is 1000Mb/s and the other is 100MB /s phy, which can be used after 1000Mb/s mode. If 100MB /s is used, it cannot be connected to the Internet. If the phy is identified as 100 Mbit /s, the transmission rate is different from that of 1000 MB /s. Is there any way to modify the driver or device tree, or any configuration, so that the network port can be identified as 1000 MB /s even when the network port is inserted into 100 Mbit /s?

0 Kudos
Reply
0 Replies