imx8mp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mp

852件の閲覧回数
qwerqq
Contributor I

Hello:

Hello:

My network port hardware is set to 1000Mb/s, and the phy is also 1000Mb/s phy. My switch has two modes, one is 1000Mb/s and the other is 100MB /s phy, which can be used after 1000Mb/s mode. If 100MB /s is used, it cannot be connected to the Internet. If the phy is identified as 100 Mbit /s, the transmission rate is different from that of 1000 MB /s. Is there any way to modify the driver or device tree, or any configuration, so that the network port can be identified as 1000 MB /s even when the network port is inserted into 100 Mbit /s?

0 件の賞賛
返信
0 返答(返信)