imx8mp scarthgap fetch error nnshark

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mp scarthgap fetch error nnshark

1,345件の閲覧回数
deepakraj
Contributor III

Hi ,

we are building scarthgap for imx8mp , we used below repo command from meta-imx .

repo init -u https://github.com/nxp-imx/imx-manifest.git -b imx-linux-scarthgap -m imx-6.6.23-2.0.0.xml

 DISTRO=fsl-imx-xwayland MACHINE=imx8mpevk source imx-setup-release.sh -b build-xwayland


when we try building image , we are facing nnshark fetch error , attached log file for reference

Resolving deltas: 100% (1839/1839), done.
Cloning into bare repository '/media/adlinkccoe29/SSD1/imx8mp/evk_imx8mp/downloads//git2/anongit.freedesktop.org.gstreamer.common'...
fatal: read error: Connection reset by peer
--2024-08-19 09:33:36-- http://downloads.yoctoproject.org/mirror/sources/git2_anongit.freedesktop.org.gstreamer.common.tar.g...
Resolving downloads.yoctoproject.org (downloads.yoctoproject.org)... 198.145.29.62
Connecting to downloads.yoctoproject.org (downloads.yoctoproject.org)|198.145.29.62|:80... connected.
HTTP request sent, awaiting response... 404 Not Found
2024-08-19 09:33:37 ERROR 404: Not Found.

--2024-08-19 09:33:37-- http://sources.openembedded.org/git2_anongit.freedesktop.org.gstreamer.common.tar.gz
Resolving sources.openembedded.org (sources.openembedded.org)... 198.145.29.27
Connecting to sources.openembedded.org (sources.openembedded.org)|198.145.29.27|:80... connected.
HTTP request sent, awaiting response... 404 Not Found
2024-08-19 09:33:38 ERROR 404: Not Found.

--2024-08-19 09:33:38-- https://mirrors.kernel.org/yocto-sources/git2_anongit.freedesktop.org.gstreamer.common.tar.gz
Resolving mirrors.kernel.org (mirrors.kernel.org)... 139.178.88.99, 2604:1380:45e3:2400::1
Connecting to mirrors.kernel.org (mirrors.kernel.org)|139.178.88.99|:443... connected.
HTTP request sent, awaiting response... 404 Not Found
2024-08-19 09:33:39 ERROR 404: Not Found.

--2024-08-19 09:33:39-- http://downloads.yoctoproject.org/mirror/sources/git2_github.com.nxp-imx.nnshark.git.tar.gz
Resolving downloads.yoctoproject.org (downloads.yoctoproject.org)... 198.145.29.62
Connecting to downloads.yoctoproject.org (downloads.yoctoproject.org)|198.145.29.62|:80... connected.
HTTP request sent, awaiting response... 404 Not Found
2024-08-19 09:33:39 ERROR 404: Not Found.

--2024-08-19 09:33:39-- http://sources.openembedded.org/git2_github.com.nxp-imx.nnshark.git.tar.gz
Resolving sources.openembedded.org (sources.openembedded.org)... 198.145.29.27
Connecting to sources.openembedded.org (sources.openembedded.org)|198.145.29.27|:80... connected.
HTTP request sent, awaiting response... 404 Not Found
2024-08-19 09:33:40 ERROR 404: Not Found.

--2024-08-19 09:33:40-- https://mirrors.kernel.org/yocto-sources/git2_github.com.nxp-imx.nnshark.git.tar.gz
Resolving mirrors.kernel.org (mirrors.kernel.org)... 139.178.88.99, 2604:1380:45e3:2400::1
Connecting to mirrors.kernel.org (mirrors.kernel.org)|139.178.88.99|:443... connected.
HTTP request sent, awaiting response... 404 Not Found
2024-08-19 09:33:41 ERROR 404: Not Found.


DEBUG: Python function base_do_fetch finished

DEBUG: Python function do_fetch finished

0 件の賞賛
返信
1 返信

1,305件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

nnshark should be downloaded into <build-directory>/downloads/git2/github.com.nxp-imx.nnshark.git/ from SRC_URI: GitHub - nxp-imx/nnshark: Live Profiler for NNStreamer

Don't see the full log, you can check over there, and might need to check your network, it seems with some issue about DEPENDS for downloading, like gstreamer.

Or you can try manually download it and make a copy of it.

 

Regards

Harvet

0 件の賞賛
返信