imx8mp pcie eye pattern test fail

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mp pcie eye pattern test fail

2,559件の閲覧回数
jiangyaqiang
Senior Contributor I

Hi :

My board PCIE eye pattern test fail at something, as bellow:

jiangyaqiang_0-1632386510915.png

The "low Limit" is a litter too fast. 

which register should I tune to pass it ?

I have attachment the complete test report.

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,548件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yaqiang

 

reason may incorrect testing measurements, may be recommended to recheck them using AN12444

PCIe Certification Guide for i.MX8 Serials

 

Best regards
igor

0 件の賞賛
返信

2,543件の閲覧回数
jiangyaqiang
Senior Contributor I

Hi igor:

 

Thanks.

I have checked the file , there is one parameter using in the file: pcie_cz_enabled=yes,

I can't find it in kernel, could you tell me what's the parameter used for ?

BTW, We have test the EVK board, it passed, any we use the same kernel and config in my board, it fail, the fail is a very little margin, so I want to know what register is relative to the fail ?

0 件の賞賛
返信