imx8mp pcie eye pattern test fail

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mp pcie eye pattern test fail

2,558 Views
jiangyaqiang
Senior Contributor I

Hi :

My board PCIE eye pattern test fail at something, as bellow:

jiangyaqiang_0-1632386510915.png

The "low Limit" is a litter too fast. 

which register should I tune to pass it ?

I have attachment the complete test report.

 

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

2,547 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yaqiang

 

reason may incorrect testing measurements, may be recommended to recheck them using AN12444

PCIe Certification Guide for i.MX8 Serials

 

Best regards
igor

0 Kudos
Reply

2,542 Views
jiangyaqiang
Senior Contributor I

Hi igor:

 

Thanks.

I have checked the file , there is one parameter using in the file: pcie_cz_enabled=yes,

I can't find it in kernel, could you tell me what's the parameter used for ?

BTW, We have test the EVK board, it passed, any we use the same kernel and config in my board, it fail, the fail is a very little margin, so I want to know what register is relative to the fail ?

0 Kudos
Reply