Hi
I am working on a custom board based on imx8mm + Yocto . I am not able to access the GPIOs through sysfs. I have a button connected to GPIO5_IO0 and LED connected to GPIO1_IO23. I am trying to turn the LED on when the button is pressed from user-space. It is not working.
I am able to export the GPIO pin in sysfs. I can change the entry in the value, it is reflecting properly. But no changes on the device. Also when the button is presses, I expect the value to change. But not happening.
Although I managed to access the LED through Linux driver, and I am trying to access the button using one of the existing driver.
I have tried similar thing with imx8mm evk + Android default image.
Tried to export the gpio connected to LED. It is not creating any directory.
evk_8mm:/sys/class/gpio # echo 80 > export
1|evk_8mm:/sys/class/gpio # ls
export gpiochip128 gpiochip496 gpiochip96
gpiochip0 gpiochip32 gpiochip64 unexport
Tried to change the brightness.
evk_8mm:/sys/class/leds/status # echo 1 > brightness
There is no change in LED brightness.
Any idea why we are not able to access the GPIO through sysfs ?
Thanks,
Avijit
 
					
				
		
GPIO5_IO00 should be either 5*32+0 = 160 or (5-1)*32+0=128, depending on what is GPIOx block numbering in your i.MX, counting from 0 (GPIO0 is the first) or counting from 1 (GPIO1 is the first). So either 160 or 128, but you do
evk_8mm:/sys/class/gpio # echo 80 > export
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Avijit
may be useful to look at below link
Best regards
igor