imx8mm Android version ECM with AG35

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mm Android version ECM with AG35

2,327件の閲覧回数
fanxiaoyun
Contributor I

imx8mm Android9 communicate with AG35 through USB, imx8mm is HOST, and AG35 (4g module ,Quectel)is slave,but there must be  something wrong with android config, cause same kernel source code in linux version works ok, but android fails.

Cdc_ether and usbnet are builtin module. Kenel log shows that usb is recognized, I manually ifconfig usb0 up and set a ip to it, but still cannot ping through it.  Error shows "unreachable network". 

kernel log :

[ 84.045145] cdc_ether 1-1.3:1.4 usb0: unregister 'cdc_ether' usb-ci_hdrc.1-1.3, CDC Ethernet Device
[ 85.801652] usb 1-1.3: new high-speed USB device number 5 using ci_hdrc
[ 85.933836] usb 1-1.3: New USB device found, idVendor=2c7c, idProduct=0435
[ 85.940731] usb 1-1.3: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ 85.948212] usb 1-1.3: Product: LTE Module
[ 85.952331] usb 1-1.3: Manufacturer: Quectel, Incorporated
[ 85.957934] usb 1-1.3: SerialNumber: ecde80c
[ 85.984406] cdc_ether 1-1.3:1.4 usb0: register 'cdc_ether' at usb-ci_hdrc.1-1.3, CDC Ethernet Device, 22:f1:41:57:a1:30

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,301件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Have you tried contacting quectel?

I see that they have an Android Driver user guide in their webpage:

https://www.quectel.com/product/lte-ag35-automotive-module

Best regards,
Aldo.

0 件の賞賛
返信

2,294件の閲覧回数
fanxiaoyun
Contributor I

Hi,

I had contacted quectel at the first time,and patch code is most about the option.c, the driver about ecm is not involved.

The "usb0" network device is already recognized,and could be assigned a ip manually.

ifconfig usb0 up

ifconfig usb0 192.168.225.3

ping 192.168.225.1  failed.  //192.168.225.1 is the ip of  AG35.

0 件の賞賛
返信