imx8m M4 GPIO_PinInit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8m M4 GPIO_PinInit

924 Views
lmcbeath
Contributor I

I am using rproc to load an image running FreeRTOS into the m4 and run.

The M4 uses GPIO_PinInit to setup SPI and gpio interrupts.

We also use some scripts on the Linux side to configure IO pins.

 

Can the M4 call GPIO_PinInit at anytime or do we need to be concerned about when the M4 calls these functions if Linux is configuring IO (for different pins) at the same time?

Labels (1)
0 Kudos
Reply
0 Replies