imx8m M4 GPIO_PinInit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8m M4 GPIO_PinInit

922件の閲覧回数
lmcbeath
Contributor I

I am using rproc to load an image running FreeRTOS into the m4 and run.

The M4 uses GPIO_PinInit to setup SPI and gpio interrupts.

We also use some scripts on the Linux side to configure IO pins.

 

Can the M4 call GPIO_PinInit at anytime or do we need to be concerned about when the M4 calls these functions if Linux is configuring IO (for different pins) at the same time?

ラベル(1)
0 件の賞賛
返信
0 返答(返信)