imx8dx, the startup process

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8dx, the startup process

1,545件の閲覧回数
songhongliang
Contributor II

HI 

         Now my board sometimes fails to start. I am troubleshooting the problem. I have opened the scfw log. When the system fails to start, there is no scfw log. When it starts normally, the scfw log is also available. My next step is What needs to be done, and then go to troubleshoot the places that may cause the system to fail to start

Thanks;

0 件の賞賛
返信
2 返答(返信)

1,539件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Hongliang

 

the ROM captures event logs through the boot process, one can look at AN12853 to find reason for failure   i.MX ROM Log Events 

 

Best regards
igor

0 件の賞賛
返信

1,535件の閲覧回数
songhongliang
Contributor II

HI

    What tool do I need to view the  ROM captures event logs

 

Thanks

0 件の賞賛
返信