imx8dx, the startup process

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8dx, the startup process

1,507 Views
songhongliang
Contributor II

HI 

         Now my board sometimes fails to start. I am troubleshooting the problem. I have opened the scfw log. When the system fails to start, there is no scfw log. When it starts normally, the scfw log is also available. My next step is What needs to be done, and then go to troubleshoot the places that may cause the system to fail to start

Thanks;

0 Kudos
Reply
2 Replies

1,501 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hongliang

 

the ROM captures event logs through the boot process, one can look at AN12853 to find reason for failure   i.MX ROM Log Events 

 

Best regards
igor

0 Kudos
Reply

1,497 Views
songhongliang
Contributor II

HI

    What tool do I need to view the  ROM captures event logs

 

Thanks

0 Kudos
Reply