imx8dx The serial port uses 115200 baud rate garbled

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8dx The serial port uses 115200 baud rate garbled

1,732 次查看
songhongliang
Contributor II

HI ,

I am using lpuart1 of imx8dx. When I set up and call lpuart1 in the app, if the baud rate is 57600, the communication can be normal. When the baud rate is 115200, garbled characters will appear. I don't know where is the problem, can you give me some help

 

thanks

0 项奖励
回复
1 回复

1,724 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Hongliang

 

reason may be uart timings, probably due to long cable/high capacitive load.

One can check it with oscilloscope using sect.4.10.15 UART I/O configuration and timing parameters

i.MX 8DualX Automotive and Infotainment Applications Processors

 

Best regards
igor

0 项奖励
回复