imx8dx 512M ddr for reserved-memory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8dx 512M ddr for reserved-memory

773件の閲覧回数
songhongliang
Contributor II

HI,

I am using imx8dx + 512M RAM,now the reserved-memory for cam  gpu How to set the size.

original:

imx8dx-mek.dts file:

linux,cma {
compatible = "shared-dma-pool";
reusable;
size = <0 0x14000000>;
alloc-ranges = <0 0x98000000 0 0x14000000>;
linux,cma-default;
};

&imx8_gpu_ss {
reg = <0x80000000 0x40000000>, <0x0 0x08000000>;
reg-names = "phys_baseaddr", "contiguous_mem";
};

 

imx8x-mek.dtsi file:

 

reserved-memory {
#address-cells = <2>;
#size-cells = <2>;
ranges;

/*
* 0x8800_0000 ~ 0x8FFF_FFFF is reserved for M4
* Shouldn't be used at A core and Linux side.
*
*/
m4_reserved: m4@0x88000000 {
no-map;
reg = <0 0x88000000 0 0x8000000>;
};

rpmsg_reserved: rpmsg@0x90000000 {
no-map;
reg = <0 0x90200000 0 0x200000>;
};

decoder_boot: decoder-boot@84000000 {
reg = <0 0x84000000 0 0x2000000>;
no-map;
};

encoder_boot: encoder-boot@86000000 {
reg = <0 0x86000000 0 0x200000>;
no-map;
};

decoder_rpc: decoder-rpc@0x92000000 {
reg = <0 0x92000000 0 0x200000>;
no-map;
};

encoder_rpc: encoder-rpc@0x92200000 {
reg = <0 0x92200000 0 0x200000>;
no-map;
};
encoder_reserved: encoder_reserved@94400000 {
no-map;
reg = <0 0x94400000 0 0x800000>;
};
/* global autoconfigured region for contiguous allocations */
linux,cma {
compatible = "shared-dma-pool";
reusable;
size = <0 0x3c000000>;
alloc-ranges = <0 0x96000000 0 0x3c000000>;
linux,cma-default;
};
};

reserved-memory {
#address-cells = <2>;
#size-cells = <2>;
ranges;

vdev0vring0: vdev0vring0@90000000 {
compatible = "shared-dma-pool";
reg = <0 0x90000000 0 0x8000>;
no-map;
};

vdev0vring1: vdev0vring1@90008000 {
compatible = "shared-dma-pool";
reg = <0 0x90008000 0 0x8000>;
no-map;
};

vdev1vring0: vdev1vring0@90010000 {
compatible = "shared-dma-pool";
reg = <0 0x90010000 0 0x8000>;
no-map;
};

vdev1vring1: vdev1vring1@90018000 {
compatible = "shared-dma-pool";
reg = <0 0x90018000 0 0x8000>;
no-map;
};

vdevbuffer: vdevbuffer {
compatible = "shared-dma-pool";
reg = <0 0x90400000 0 0x100000>;
no-map;
};
};

 

 

thanks,

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

765件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi songhongliang

 

for cma size there is no some formula, it can be found experimentally for

each configuration, try some heavy load use cases for example described in

AN12338  sect.4.2.2. Kanzi

i.MX 8QuadXPlus Power Consumption Measurement

 

Best regards
igor

0 件の賞賛
返信

761件の閲覧回数
songhongliang
Contributor II

HI,

For example, a simple QT application for automotive instrumentation, using LVDS display, how much GPU reserved memory needs to be set

Thanks

0 件の賞賛
返信

772件の閲覧回数
songhongliang
Contributor II

HI,

I use one lvds lcd and three AHD camera。

thanks!

0 件の賞賛
返信