imx8dx 512M ddr for reserved-memory

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8dx 512M ddr for reserved-memory

726 次查看
songhongliang
Contributor II

HI,

I am using imx8dx + 512M RAM,now the reserved-memory for cam  gpu How to set the size.

original:

imx8dx-mek.dts file:

linux,cma {
compatible = "shared-dma-pool";
reusable;
size = <0 0x14000000>;
alloc-ranges = <0 0x98000000 0 0x14000000>;
linux,cma-default;
};

&imx8_gpu_ss {
reg = <0x80000000 0x40000000>, <0x0 0x08000000>;
reg-names = "phys_baseaddr", "contiguous_mem";
};

 

imx8x-mek.dtsi file:

 

reserved-memory {
#address-cells = <2>;
#size-cells = <2>;
ranges;

/*
* 0x8800_0000 ~ 0x8FFF_FFFF is reserved for M4
* Shouldn't be used at A core and Linux side.
*
*/
m4_reserved: m4@0x88000000 {
no-map;
reg = <0 0x88000000 0 0x8000000>;
};

rpmsg_reserved: rpmsg@0x90000000 {
no-map;
reg = <0 0x90200000 0 0x200000>;
};

decoder_boot: decoder-boot@84000000 {
reg = <0 0x84000000 0 0x2000000>;
no-map;
};

encoder_boot: encoder-boot@86000000 {
reg = <0 0x86000000 0 0x200000>;
no-map;
};

decoder_rpc: decoder-rpc@0x92000000 {
reg = <0 0x92000000 0 0x200000>;
no-map;
};

encoder_rpc: encoder-rpc@0x92200000 {
reg = <0 0x92200000 0 0x200000>;
no-map;
};
encoder_reserved: encoder_reserved@94400000 {
no-map;
reg = <0 0x94400000 0 0x800000>;
};
/* global autoconfigured region for contiguous allocations */
linux,cma {
compatible = "shared-dma-pool";
reusable;
size = <0 0x3c000000>;
alloc-ranges = <0 0x96000000 0 0x3c000000>;
linux,cma-default;
};
};

reserved-memory {
#address-cells = <2>;
#size-cells = <2>;
ranges;

vdev0vring0: vdev0vring0@90000000 {
compatible = "shared-dma-pool";
reg = <0 0x90000000 0 0x8000>;
no-map;
};

vdev0vring1: vdev0vring1@90008000 {
compatible = "shared-dma-pool";
reg = <0 0x90008000 0 0x8000>;
no-map;
};

vdev1vring0: vdev1vring0@90010000 {
compatible = "shared-dma-pool";
reg = <0 0x90010000 0 0x8000>;
no-map;
};

vdev1vring1: vdev1vring1@90018000 {
compatible = "shared-dma-pool";
reg = <0 0x90018000 0 0x8000>;
no-map;
};

vdevbuffer: vdevbuffer {
compatible = "shared-dma-pool";
reg = <0 0x90400000 0 0x100000>;
no-map;
};
};

 

 

thanks,

0 项奖励
回复
3 回复数

718 次查看
igorpadykov
NXP Employee
NXP Employee

Hi songhongliang

 

for cma size there is no some formula, it can be found experimentally for

each configuration, try some heavy load use cases for example described in

AN12338  sect.4.2.2. Kanzi

i.MX 8QuadXPlus Power Consumption Measurement

 

Best regards
igor

0 项奖励
回复

714 次查看
songhongliang
Contributor II

HI,

For example, a simple QT application for automotive instrumentation, using LVDS display, how much GPU reserved memory needs to be set

Thanks

0 项奖励
回复

725 次查看
songhongliang
Contributor II

HI,

I use one lvds lcd and three AHD camera。

thanks!

0 项奖励
回复