imx8 raw camera

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8 raw camera

2,743 Views
jhongting
Contributor II

I used yocto sw 4.9.5.1-ga sw test raw camera always fail.

gst-launch-1.0 and gst-device-monitor-1.0 tool , are can't detect my raw sensor camera (imx219), the camera via csi output format set to SRGGB-10 (RG10) 

May I ask NXP have any porting raw sensor doc guide on imx8? 

0 Kudos
Reply
1 Reply

1,972 Views
igorpadykov
NXP Employee
NXP Employee

Hi ben

supported cameras and formats are described in AN12187 Quick Start Guide

for MINISASTOCSI for i.MX 8M Evaluation Kit

https://www.nxp.com/docs/en/application-note/AN12187.pdf 

Unfortunately porting raw sensor doc guide on imx8 currently not available, sorry.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply