imx8-prg 56070000.prg: unsupported crop line 720 for modifier 0x0000000000000000

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8-prg 56070000.prg: unsupported crop line 720 for modifier 0x0000000000000000

802 次查看
shalanyang
Contributor II

HI ,

    we are use imx8qxp ,when I use lvds show logo,the picture can show ,but have some error msg,follow:

    
[ 9.715977] imx8-prg 56070000.prg: unsupported crop line 720 for modifier 0x0000000000000000
[ 9.785750] imx8-prg 56070000.prg: unsupported crop line 720 for modifier 0x0000000000000000
[ 9.851739] imx8-prg 56070000.prg: unsupported crop line 720 for modifier 0x0000000000000000
[ 9.917742] imx8-prg 56070000.prg: unsupported crop line 720 for modifier 0x0000000000000000
[ 9.983571] imx8-prg 56070000.prg: unsupported crop line 720 for modifier 0x0000000000000000
[ 10.049798] imx8-prg 56070000.prg: unsupported crop line 720 for modifier 0x0000000000000000
[ 10.116146] imx8-prg 56070000.prg: unsupported crop line 720 for modifier 0x0000000000000000

I found it print in drivers/gpu/imx/imx8_dprc.c 

void prg_configure(struct prg *prg, unsigned int width, unsigned int height,
unsigned int x_offset, unsigned int y_offset,
unsigned int stride, unsigned int bits_per_pixel,
unsigned long baddr, u32 format, u64 modifier,
bool start)

{

...............

if (y_offset >
((format == DRM_FORMAT_NV21 || format == DRM_FORMAT_NV12) ?
(PRG_HANDSHAKE_8LINES - 1) : (PRG_HANDSHAKE_4LINES - 1))) {
dev_err(prg->dev,
"unsupported crop line %d for modifier 0x%016llx\n",
y_offset, modifier);
return;
}

.......

}

BSP Version: body#

imx_4.9.51_8qxp_beta

why have this errr msg?

TKS

0 项奖励
回复
3 回复数

602 次查看
shalanyang
Contributor II

HI ,igorpadykov,

      Sorry ,we use the BSP Version is L4.9.51_8qm-beta2/8qxp-beta ,the problem is exist ?can you help me?

      

0 项奖励
回复

602 次查看
igorpadykov
NXP Employee
NXP Employee

Hi shalan

please try beta2 release, follow suggestion on

How to enable the HDMI for IMX8 QXP MEK with LVDS to HDMI converter 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

602 次查看
shalanyang
Contributor II

IMX8QXP 

0 项奖励
回复