imx8-prg 56070000.prg: unsupported crop line 720 for modifier 0x0000000000000000

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8-prg 56070000.prg: unsupported crop line 720 for modifier 0x0000000000000000

764件の閲覧回数
shalanyang
Contributor II

HI ,

    we are use imx8qxp ,when I use lvds show logo,the picture can show ,but have some error msg,follow:

    
[ 9.715977] imx8-prg 56070000.prg: unsupported crop line 720 for modifier 0x0000000000000000
[ 9.785750] imx8-prg 56070000.prg: unsupported crop line 720 for modifier 0x0000000000000000
[ 9.851739] imx8-prg 56070000.prg: unsupported crop line 720 for modifier 0x0000000000000000
[ 9.917742] imx8-prg 56070000.prg: unsupported crop line 720 for modifier 0x0000000000000000
[ 9.983571] imx8-prg 56070000.prg: unsupported crop line 720 for modifier 0x0000000000000000
[ 10.049798] imx8-prg 56070000.prg: unsupported crop line 720 for modifier 0x0000000000000000
[ 10.116146] imx8-prg 56070000.prg: unsupported crop line 720 for modifier 0x0000000000000000

I found it print in drivers/gpu/imx/imx8_dprc.c 

void prg_configure(struct prg *prg, unsigned int width, unsigned int height,
unsigned int x_offset, unsigned int y_offset,
unsigned int stride, unsigned int bits_per_pixel,
unsigned long baddr, u32 format, u64 modifier,
bool start)

{

...............

if (y_offset >
((format == DRM_FORMAT_NV21 || format == DRM_FORMAT_NV12) ?
(PRG_HANDSHAKE_8LINES - 1) : (PRG_HANDSHAKE_4LINES - 1))) {
dev_err(prg->dev,
"unsupported crop line %d for modifier 0x%016llx\n",
y_offset, modifier);
return;
}

.......

}

BSP Version: body#

imx_4.9.51_8qxp_beta

why have this errr msg?

TKS

0 件の賞賛
返信
3 返答(返信)

564件の閲覧回数
shalanyang
Contributor II

HI ,igorpadykov,

      Sorry ,we use the BSP Version is L4.9.51_8qm-beta2/8qxp-beta ,the problem is exist ?can you help me?

      

0 件の賞賛
返信

564件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi shalan

please try beta2 release, follow suggestion on

How to enable the HDMI for IMX8 QXP MEK with LVDS to HDMI converter 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

564件の閲覧回数
shalanyang
Contributor II

IMX8QXP 

0 件の賞賛
返信